Solution


Crude Oil Weighing

A weighing system is needed to measure mass amounts of crude oil.


Summary

  • Customer Need / Challenge

    When oil is extracted from the ground, a refinement process follows to remove sediments and other impurities. After the filtering process, the crude oil needs to be weighed in order to be redistributed. A weighing system is needed to measure mass amounts of crude oil. 

  • Interface Solution

    Interface’s solution is to secure four SSB Sealed Beam Load Cells at the bottom of a metal platform. The SSB Sealed Beam Load Cells will measure the force applied by the weight of the barrels of crude oil. All four SSB’s are connected to a JB104SS Junction Box, which is connected to the 480 Bidirectional Weight Indicator, and combined the accurate weight results are displayed.

  • Results

    Interface’s industrial weighing system accurately weighed the barrels of crude oil, so it can move onto the next process of distribution.

Materials


  • Four SSB Sealed Beam Load Cells

  • JB104SS Junction Box

  • 480 Bidirectional Weight Indicator

How it Works


  1. Four SSB Sealed Beam Load Cells are secured to the bottom of a metal platform.

  2. Barrels of crude oil are placed on the Interface’s industrial scale, where it was weighed on the metal platform.

  3. The multiple SSB’s were wired together to a JB104SS Junction Box, which was then connected to the 480 Bidirectional Weight Indicator to measure the combined results of the four SSB Sealed Beam Load Cells.

Download PDF